Understand bxCAN TX mailbox
Hi all
I want to understand behavior of TX mailbox here I am trying to send three ID but only i able to see two ID at a time in TI0R. I have fewer doubts which I hope you can clear.
Doubt 1: Do I have to use three different mail box for three ID or One is enough .
Doubt 2. Like in RX mailbox I have locking mechanism in which I can see different RX frame in RXFIFO0 so I mean to say It can hold upto three different messages. So is there any logic in TX mailbox also to locked or to see all ID because I think it is overwriting the buffer.
CAN_TxHeaderTypeDef txHeader;
uint8_t tx_data[8] = {0x11, 0x22, 0x33, 0x44, 0x55, 0x66, 0x77, 0x88};
uint32_t tx_mailbox_used;
txHeader.StdId = 0x3e8; // Example CAN ID
txHeader.RTR = CAN_RTR_DATA;
txHeader.IDE = CAN_ID_STD;
txHeader.DLC = 8;
if (HAL_CAN_AddTxMessage(&hcan1, &txHeader, tx_data, &tx_mailbox_used) != HAL_OK)
{
Error_Handler();
}
txHeader.StdId = 0x2bc; // Example CAN ID
txHeader.RTR = CAN_RTR_DATA;
txHeader.IDE = CAN_ID_STD;
txHeader.DLC = 8;
if (HAL_CAN_AddTxMessage(&hcan1, &txHeader, tx_data, &tx_mailbox_used) != HAL_OK)
{
Error_Handler();
}
txHeader.StdId = 0x100; // Example CAN ID
txHeader.RTR = CAN_RTR_DATA;
txHeader.IDE = CAN_ID_STD;
txHeader.DLC = 8;
if (HAL_CAN_AddTxMessage(&hcan1, &txHeader, tx_data, &tx_mailbox_used) != HAL_OK)
{
Error_Handler();
}
HAL_Delay(1000);
}
B.R
Ashish