Skip to main content
Explorer II
August 22, 2024
Solved

Understanding on Flash Memory Endurance Cycles for STM32 Microcontrollers

  • August 22, 2024
  • 2 replies
  • 3705 views

I’m using an STM32 microcontroller and am trying to understand more about the flash memory endurance cycles. The datasheet mentions an endurance of 1 kcycle (1,000 program/erase cycles). I think possible Write and read  (1000 cycles ) or is there any limits about  program/erase cycles?

Could  explain what exactly this means in terms of practical use? How are these cycles characterized, and what factors might affect the actual endurance in a real-world application?

 

 

 

Thanks!"

    This topic has been closed for replies.
    Best answer by TDK

    1 cycle = 1 erase + 1 write.

    That means the chip will work if you erase and program it 1000 times. After that, operation is not guaranteed (but it's likely to continue to work well after that point).

     

    The STM32G0x0 is a budget line. Lots of other families have 10k endurance cycles. If you have an application with lots of writing, perhaps look for a chip with higher endurance, or use an external dedicated FLASH chip.

    2 replies

    TDKAnswer
    Super User
    August 22, 2024

    1 cycle = 1 erase + 1 write.

    That means the chip will work if you erase and program it 1000 times. After that, operation is not guaranteed (but it's likely to continue to work well after that point).

     

    The STM32G0x0 is a budget line. Lots of other families have 10k endurance cycles. If you have an application with lots of writing, perhaps look for a chip with higher endurance, or use an external dedicated FLASH chip.