Understanding Power Consumption using SMPS on STM32N6
I am unsure if I correctly understand the power consumption of the N6 Family.
I want to supply the MCU with 1,8V and use the internal SMPS to supply Core with 0,81V.
When it comes to designing the 1,8V voltage source, how much current do I have to expect?
Datasheet chapter 5.3.6 details supply current characteristics
- I see that I_DD is almost negligable in the grand scheme (less than 1 mA)
- CORE supplied by SMPS is given as current I_DDA1V8, order of magnitude around 100mA typ
- I_DDA1V8 in and of itself also quite small with around 5 mA
- I_DDA1V8AON itself also around 5 mA
- Table 39. shows current consumption of SMPS, the given current is also I_DDA1V8AON with values up to 100 mA typ.
Since some currents are defined multiple times in different tables I am having trouble to understand which values to take for a maximum current calculation.
Do I have to add all together?
Also, CORE supply without SMPS through I_DDCORE needs less current than when supplied with SMPS through I_DDA1V8 (most of the scenarios at least). I am having trouble to understand how that makes sense, since V_CORE is less than half of 1.8V. I would expect the SMPS to draw less current.
I guess there is one detail or understanding that I am missing.
I just finished reading AN5967 but that didn't help.
Please advise me on how to deduce maximum current consumption when using SMPS.
Thanks
Lucas