Unexpected RTC Alarm IRQs after PRER adjustment on STM32G0 (RTC running on LSI)
I’m working with an STM32-based system where the RTC is running on the internal LSI. My goal is to maintain reasonable time accuracy (within a few seconds) while periodically receiving the correct world time over an external communication interface.
To do this, I preset the expected LSI frequency and continuously calibrate it based on time updates I receive. This logic seems to be working well. However, I'm encountering an issue where the RTC alarm interrupt triggers unexpectedly after modifying the `PRER` (prescaler) register — even though the alarm is configured to trigger only once per minute.
Below is the code I'm using to adjust the `PRER` value (executed from within the RTC alarm IRQ):
hrtc.State = HAL_RTC_STATE_BUSY;
__HAL_RTC_WRITEPROTECTION_DISABLE(&hrtc);
status = RTC_EnterInitMode(&hrtc);
if (status == HAL_OK) {
hrtc.Instance->PRER = synchPrediv;
hrtc.Instance->PRER |= (asynchPrediv << RTC_PRER_PREDIV_A_Pos);
print("[RTC] - DR:%08X, TR:%08X\n", (hrtc.Instance->DR), (hrtc.Instance->TR));
status = RTC_ExitInitMode(&hrtc);
}
__HAL_RTC_WRITEPROTECTION_ENABLE(&hrtc);
if (status == HAL_OK) {
hrtc.State = HAL_RTC_STATE_READY;
}
Here is an example of the logs observed during runtime:
```
13:23:59.063303 [RTC] - Intended 32513(60|532) freq. corrected to 34138(100|337) to drop 3 difference.
13:23:59.063511 [RTC] - DR:00252528, TR:00132400
13:23:59.063854 [Time] - System date/time: 2025-05-28 13:24:00
13:24:00.109324 [RTC] - freq. set to 32513(60|532).
13:24:00.109532 [RTC] - DR:00252528, TR:00132400
13:24:00.109614 [Time] - System date/time: 2025-05-28 13:24:00
13:24:01.106327 [Time] - System date/time: 2025-05-28 13:24:00
```
Context:
- Lines prefixed with [RTC] are printed when PRER is updated.
- Lines prefixed with [Time] come from the alarm IRQ, which fires every minute.
- The alarm logic has three modes:
- simple IRQ: default minute alarm.
- time catch period enter: triggered when we need to speed up or slow down time.
- time catch period exit: used to restore previously calculated frequency.
Expected behavior:
time catch period enter → ~1 minute later → time catch period exit → 1 minute later → simple IRQ→ 1 minute later → simple IRQ→ ....
Actual behavior:
Sometimes, two or all three trigger within the same second or a few seconds of each other. Apart IRQ's which modifies PRER - no such behavior is observed.
My Question:
What could be causing the RTC alarm to behave unpredictably or trigger early after modifying PRER?
Is it possible that modifying PRER causes an internal resynchronization that affects the alarm trigger logic?
Any insights or similar experiences are greatly appreciated.
Thank you in advance,
Laurynas