Usage of ULPI & CANFD interfaces
I want to use the ULPI interface & both the CAN interface for my project
But I see
For USB:
Pin No: 194 pin name: PB5 Module function : USB_OTG_HS_ULPI_D7, ONLY ONE PIN no other pins are there
For CAN
Pin No: 194,195 pin name: PB5,PB6 Module function : CAN2_RX,CAN2_TX
Pin No: 104,105 pin name: PB12,PB13 Module function : CAN2_RX,CAN2_TX
How to proceed with it, since we have clash with Pin No 194?