USB available on STM32G0B0KET6 ?
DS13565 Rev 2 says under 3.20: "The embedded USB controller cannot be used on STM32G0B0KE as this device does not provide an HSE oscillator input.". Well, sounds reasonable. But same DS says in Table 11 for Pin 2 (LQFP32) PC14: "OSC32_IN, OSC_IN" whereas for the higher pin count packages PC14 has only "OSC32_IN".
So, HSE bypass is available on LQFP32?!
Now CubeMX 6.10.0 with G0 1.6.1, gives after selection of "G0 series" and "USB FS" a list *INCLUDING* STM32G0B0KET6, and even the "Features" tab of the very same device shows "USB 2.0 FS device and host controller". After selecting STM32G0B0KET6, one can definitely check "BYPASS Clock Source" under "RCC", and Pinout view shows this is located on PC14, as expected. Clock config tab now allows HSE -> PLL -> PLLR -> SYSCLOCK, and even shows "PLLQ" and "USB Clock Mux", but both not configurable. But neither RM nor DS restricts use of PLLQ divider for LQFP32. Pretty inconsistent.
So, after all, what's the intention regarding USB on STM32G0B0KET6?