Question
usb buffer descriptor masks in cmsis device h5
They are defined like this in stm32h563xx.h:
/*Buffer Descriptor Mask*/
#define USB_PMA_TXBD_ADDMSK (0xFFFF0000UL)
#define USB_PMA_TXBD_COUNTMSK (0x0000FFFFUL)
#define USB_PMA_RXBD_ADDMSK (0xFFFF0000UL)
#define USB_PMA_RXBD_COUNTMSK (0x03FFFFFFUL)ADDMSKs are correct, but I was expecting both COUNTMSK to be 0xFC00FFFFUL since both COUNT_TX and COUNT_RX are 10 bits [25:16]. When double buffering is used there is BLSIZE and NUM_BLOCK but I dont see anything about these in the header. Is there a reason the TXBD and RXBD_COUNTMSK are defined like this ?