usb driver for STM32373C-EVAL evaluation board for windows 10
i am working with The STM32373C-EVAL evaluation board which has a STM32F373VCT6 microcontroller. i have the task to read the adc data via usb interface. the usb interface is not working (nothing is shown on the pc that a device is connected). i searched the usb driver on stm32 website, it says in STSW-STM32102 that the driver is only for windows 7 and 8. but i am using windows 10 and can't find a usb driver for it. does anyone have a solution ?