Skip to main content
Visitor II
August 25, 2025
Question

USB HS CDC stop working if Internal IP DMA is enabled on STM32F469NI

  • August 25, 2025
  • 0 replies
  • 230 views

Hi,

I am working on STM32F469NI using the USB OTG HS peripheral in CDC (VCOM) mode.

  • When using USB CDC without DMA, the VCOM works fine.

  • However, when I enable Internal IP DMA (from CubeMX → USB_OTG_HS → Parameter Settings → Enable internal IP DMA), the USB CDC communication stops working after some time.

Setup details:

  • MCU: STM32F469NI

  • USB mode: Device (CDC VCOM)

  • PHY: Internal FS PHY

  • DMA Mode: Internal IP DMA enabled for USB_OTG_HS

  • Running on custom board

Observed behavior:

  • On PC, the VCOM port is detected correctly.

  • Initially, data transfer works fine.

  • After some time (or after repeated Tx/Rx), the communication hangs completely. No data transfer occurs until reset.

  • If I disable Internal IP DMA, the issue goes away.

What I tried:

  • Checked buffer alignment (made Tx buffers 4-byte aligned).

  • Verified HAL callbacks (CDC_Transmit_FS etc.) are still being called.

Questions:

  1. Is Internal IP DMA for USB HS CDC fully supported on STM32F469NI?

  2. Are there known limitations / errata related to this?

  3. Any additional configuration needed for DMA mode (buffer alignment, cache maintenance, etc.)?

  4. Could this be an issue in Cube/HAL implementation?

Any guidance or reference examples would be helpful.

    This topic has been closed for replies.