Question
USB Library with device having multiple interfaces
Posted on October 22, 2016 at 04:27
I am not sure if this is a bug fix or an enhancement.
I am developing on a proprietary board using the STM32F7 series processor. I have a device connected via USB using the USB Host Library. This particular device has more than just a CDC interface and the CDC is NOT the first one in the descriptor list. The USB Library source file usbh_core.c has code which should be looking through all of the interfaces, but only looks at the first. To fix this, I changed this:case HOST_CHECK_CLASS:
if (phost->ClassNumber == 0)
{
USBH_UsrLog(''No Class has been registered.'');
}
else
{
phost->pActiveClass = NULL;
for (idx = 0; idx <
USBH_MAX_NUM_SUPPORTED_CLASS
; idx++)
{
if ((phost->pClass [ idx ]->ClassCode == phost->device.CfgDesc.Itf_Desc [ 0 ].bInterfaceClass))
{
phost->pActiveClass = phost->pClass [ idx ];
}
} to this:
case HOST_CHECK_CLASS:
if (phost->ClassNumber == 0)
{
USBH_UsrLog(''No Class has been registered.'');
}
else
{
phost->pActiveClass = NULL;
for (idx = 0; idx <
USBH_MAX_NUM_SUPPORTED_CLASS
; idx++)
{
for (int
infx
=
0
; infx < USBH_MAX_NUM_INTERFACES; infx++)
{
if ((phost->pClass [ idx ]->ClassCode == phost->device.CfgDesc.Itf_Desc [ infx ].bInterfaceClass))
{
phost->pActiveClass = phost->pClass [ idx ];
break;
}
}
} This picks up all of the interfaces in the descriptor.
I also modified usbh_cdc.c in the
static USBH_StatusTypeDef USBH_CDC_InterfaceInit(USBH_HandleTypeDef *phost) function to return separate notification and data interfaces. Worked out well in the long run.
You should also change the SetLineCoding and GetLineCoding functions - and maybe a couple of others - so that the ''0'' interface is not the default interface. Use the current interface.
I spent a week wondering why everything worked great over the base/notification interface but terrible on the data interfaces.
Discovered the problem tonight.
In usbh_core.c
uint8_t USBH_FindInterface(USBH_HandleTypeDef *phost, uint8_t Class, uint8_t SubClass, uint8_t Protocol, int8_t startWith)
{
USBH_InterfaceDescTypeDef *pif;
USBH_CfgDescTypeDef *pcfg;
int8_t if_ix = startWith; //0; <-- was searching from the first interface for the associated data interface - should start from current interface So, references to this function need an extra parameter for setting a starting index. The bug here is that the function was always returning the data interface for the first interface when I needed it from the next interface pair after the first.
Hope this helps people who are using USB devices with multiple interfaces or fixes a bug in the library.
#!stm32-!usb-!library-!interfaces