USB OTG_HS_VBUS on STM32H series
Hi,
I have a question about whether or not the USB VBUS connection needs to be made to the micro on the STM32H series micros (in particular the STM32H725) when operating the USB in device mode.
We are using a USB-C type connection, so we have an independent IC which performs OTG host/device detection based on the USB-C VBUS and CC1, CC2 USB-C pins, but it is not clear whether we also need to connect the VBUS to the micro's OTG_HS_VBUS pin (PA9 on this micro) to start the comms sequence when the micro is a device.
On previous STM32F series micros I believe it was mandatory to make this connection because it powered the USB transceiver but I'm not sure that this is still the case on the STM32H micros, or whether the new USB regulator can somehow be used to perform this instead (or is that just for host mode)?
Thanks for any help you can give with this.
Steve