Use of external oscillator input
Hi i am using STM32G474VET3 controller having below clock input range
– 4 to 48 MHz crystal oscillator
i am using 16 MHz right now.
What is the significance if i use 32 MHz crystal or increase my crystal value.
Does it increase speed for instruction execution . as max is 170MHz (i guess nby internal PLL)
The STM32G473xB/xC/xE devices are based on the high-performance Arm® Cortex®-M4
32-bit RISC core. They operate at a frequency of up to 170 MHz.