Using 1TB SD Card with SDMMC Interface on STM32 – Need Adapter Recommendations
Hello everyone,
I am currently working on a project using an STM32H753ZI, and I'm exploring the integration of a 1TB SD card using the SDMMC interface. I have successfully managed to write to a 32GB SD card using an SPI adapter, but I'm looking to upgrade in terms of capacity and interface speed. I would appreciate some guidance on a few points:
Compatibility: Has anyone successfully used a 1TB SD card with an STM32? Are there any specific settings or considerations I need to be aware of for compatibility, especially concerning the SDXC standard and filesystems?
Adapter Recommendations: Can anyone recommend a suitable SD card adapter that works well with STM32 for such high-capacity cards? I'm looking for something reliable for continuous read/write operations.
Performance Tips: Any tips on optimizing performance when using SDMMC with high-capacity SD cards would also be greatly appreciated.