Using QSPI PSRAM with a STM32-H753 is that possible?
Hello,
I am in the process of designing a product which is based on the STM32-H753 and requires P/SRAM.
However, I'm concerned the H753 might not support on PSRAM with QSPI, I need the PSRAM for write/read.
I haven't found any application notes or examples from ST showing connection QSPI PSRAM into the STM32 only for FMC or OCTOSPI Flash.
Has anyone successfully used QSPI PSRAM with STM32H7 ?
Are the specific requirements or limitation I should be aware of ?
(attached reference images for context):