Using SPI with DMA
Hi All, I'm using an STM32F1 with a 240x240 LCD screen that comunicates with the micro by SPI (with DMA). The screen uses the ST7789 driver (I supose it is not important). I'm working with RGB565 color format.
The problem that I have is, for example, when I'm using the ST7789_Fill_Color(YELLOW); the SPI uses the DMA and the LCD shoul be yellow but it's not. If yellow is 0b1111 1111 1110 0000 the DMA only sends to SPI the LSB (0b0000 0000 1110 0000) witch is a wrong color.
When I do the same without DMA it work's fine!
The DMA is configures this way:

I tried every configuration possible but nothing works. My question is why the DMA only graps the first byte of a color and what I have to change in order to send the real color.
Thanks in advance!!!