Using STM32H562ZI with I3C v1.0 compatible I3C Target endpoint
Hi,
I'm planning to use STM32H562ZI as I3C controller with an I3C v1.0 compatible Target endpoint. Since STM32 I3C IP supports I3C v1.1.1, will there be any potential issues on RSTDAA, ENTDAA, I3C Private Write, I3C Private Read or other electrical parameters with v1.0 ? Though I do not see any limitation based on v1.0 & v1.1.1 specifications (Apart from IBI mandatory byte and new CCCs), I'd like to hear from the community. Appreciate the help.
Thanks,
Srinath