Variable address in memory is changing when reading I2C1 CR2 register. STM32H503CBU6.
Setup Info:
Compiler: IAR EW for Arm 9.50.1, Debug build configuration, High optimization
Micro: STM32H503CBU6
I am running into an issue where when I am trying to copy the CR2 register from I2C1, it copies the wrong value and the addresses of my other variables change.
Before attempt to copy CR2, here's the register values and variable values and addresses:

After stepping over this line, this is what I am seeing for the variable values and addresses:

As you can see, not only is the copied value of CR2 wrong (should be 0 after clearing the specified bits), but the values and locations of my other variables have changed as well. Please note that I2c[m_HalIndex] is the same as I2C1; I have it defined in a header file elsewhere. Putting I2C1 explicitly was part of debugging what could be going on.
I haven't seen this sort of issue before. The code I am using was working on a STM32G071, and I've switched to the H503 because of the faster clock speed. Any guidance on this would be much appreciated. Please let me know if you need any more information, but be advised, this is part of a company project so I can only share so much.
Thank you!