VBAT on STM32U5G9J-DK1
Hello,
I have got an STM32U5G9J-DK1 and I want to use its VBAT pin which has been connected to the signal VDD_MCU, which is internal to the board, via solder bridge SB29. As far as my understanding of the data sheet goes, the VBAT pin is supposed to be fed with 1.8 V. So, I was thinking to remove the solder bridge and connect an appropriate battery for this operation. Could you suggest me some good batteries that would suffice this requirement?
Thanks in advance.
Regards,
Gaurav.