VBus triggered by Data pins STM32H743?
I have a board that uses the H743 and have been having major problems with the USB side of things. I've only just realised that I left VBus floating all this time, so I'm assuming that's a major cause of my issues..
The board I have is designed as a solder on stamp, and has a fixed 5v input that powers multiple LDOs etc. The problem lies in that I don't really want to sacrifice one of my castellated edge pins for vbus sensing, but the stamp isn't always connected to USB so I cant simply connect VBUS to 3.3v, can I?
The board is always "Self Powered", ie the 5v from USB is not directly connected to the main power in. Is there any way to trigger the VBUS pin only using the data lines?