Voltage reference buffer (VREFBUF) in U545 packages
In the Datasheet it says:
"The VREF+ pin is double-bonded with VDDA on some packages. In these packages the
internal voltage reference buffer is not available."
Does this implicitly mean all packages which do not explicitly have a VREF+ pin can not use this peripheral or are there some inbetweens (which ones) which can use internal references, just not external ones?
I'm especially surprised that even the high pin count WLCSP variant does not have such a pinout, so the smallest package to even use that (imo very useful) feature would be a "huge" 7x7mm BGA Chip.