Voltage Sense with multichannel ADC DMA
Hello everyone,
I have designed my own card and used F103 uC on it. I want to measure battery voltage with DMA method. I hope to drive BLDC motor with this card one day :) So i need to measure phase voltages and BUS battery voltage. Due to speed issues, i thought DMA would be much better option.
So, forget about the phase voltages first. I just want to sense battey voltage. I have defined some variables. I have voltage driver on the same line so i need to multiply every array value with multiplier. I eant to write buffer values to data array for true measurement of the voltage. Then i want to send this scaled values to my computer.
#define Buffer_Size 5
uint16_t V_BATT_ADC_Buffer[Buffer_Size]={0};
uint16_t V_BATT_ADC_Data[Buffer_Size]={0};
float V_BATT_ADC = 0.0;
float V_BATT = 0.0;
uint8_t V_BATT_Sense_Conv_End = 0;
float multiplier_V_BATT = (3.3/4095)*(100+5.6)/5.6;
void multiplyArray(uint16_t *array, size_t size, float multiplier) // Array multiplication function
{
for (size_t i = 0; i < size; i++)
{
array[i] = (uint16_t)(array[i] * multiplier);
}
}
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc) // Get value with DMA and write it when Conv. Cmp. to other array function
{
if (hadc == &hadc3)
{
for(int i = 0 ; i<Buffer_Size; i++)
{
V_BATT_ADC_Data[i] = V_BATT_ADC_Buffer[i];
}
V_BATT_Sense_Conv_End=1;
}
}
int main(void)
....
....
HAL_ADC_Start_DMA(&hadc3, (uint32_t *)V_BATT_ADC_Buffer, Buffer_Size);
while(1)
........
........
if(V_BATT_Sense_Conv_End == 1)
{
size_t size = sizeof(V_BATT_ADC_Buffer)/sizeof(V_BATT_ADC_Buffer[0]);
multiplyArray(V_BATT_ADC_Buffer, size, multiplier_V_BATT);
char str[80];
int V_BATT_txlength = sprintf(str, "ADC Value: %d, Battery Voltage Level: %dV\r\n", V_BATT_ADC_Data[0], V_BATT_ADC_Data[1]);
HAL_UART_Transmit(&huart1, (uint8_t*)str, V_BATT_txlength, 100);
HAL_Delay(500);
V_BATT_Sense_Conv_End=0;
}
}
As summary, i want to sense battery voltage with dma then write it to an array then multiply this array according to my voltage divider and send it to my computer. I know it is little long but any help would be appreciated.