VREF+ exceeding VDDA during power on/off
I'm trying to understand the following excerpts from the STM32L476 datasheet, which seem to contradict:
In Table 20 - the absolute maximum voltage on the VREF+ pin is given as 4.0V (VREF+ I assume falls under the "other" category).

Table 76 seems to indicate that VREF+ can never exceed VDDA. Does this include during power on and power off, or is this just a steady-state condition to satisfy the accuracy performance of the ADC? And if the latter, is it fair to assume that VREF+ can be as high as 4V, even if VDDA is 0V, as Table 20 would suggest?