VREF Internal voltage reference G431 series
Hello,
Can anyone suggest whether or not I need to connect external capacitors to the VREF+ pin if I plan to use VREF only for the onboard DAC?
Could this be a hardware problem?
STM32G431CBT6. The problem is that on the oscillogram I see oscillations with an amplitude of approximately 490 mV on the VREF+ pin. This is when Scale 2 is set to 2.9 V. If I reduce to 2.5V, the swing will be almost 1V overall. Nothing but the 1:10 oscilloscope probe is connected to the VREF+ pin on the board.
Below are the screenshots.