W25Q cannot read ID
Hello!
I have a W25Q128JVIQ connected to an STM32F446RE like the following:

I am trying to use QuadSPI in Dual Mode, but I am having difficulties reading ANY data, like the Device ID (ABh). This is my code:
W25Q_STATE W25Q_ReadID(u8_t *buf)
{
QSPI_CommandTypeDef com;
com.InstructionMode = QSPI_INSTRUCTION_1_LINE; // QSPI_INSTRUCTION_...
com.Instruction = W25Q_FULLID_DUAL_IO; // Command
com.AddressMode = QSPI_ADDRESS_1_LINE;
com.AddressSize = QSPI_ADDRESS_24_BITS;
com.Address = 0x0U;
com.AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;
com.AlternateBytes = QSPI_ALTERNATE_BYTES_NONE;
com.AlternateBytesSize = QSPI_ALTERNATE_BYTES_NONE;
com.DummyCycles = 0;
com.DataMode = QSPI_DATA_1_LINE;
com.NbData = 1;
com.DdrMode = QSPI_DDR_MODE_DISABLE;
com.DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;
com.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;
if (HAL_QSPI_Command(&hqspi, &com, HAL_QSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
return W25Q_SPI_ERR;
}
if (HAL_QSPI_Receive(&hqspi, buf, HAL_QSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
return W25Q_SPI_ERR;
}
return W25Q_OK;
}
I also tried to read instruction 92h with datamode and address mode set to DATA_2_LINES, but it returns the same.

I am pretty sure, this is not the ID, it should return 23 or 238 according to the datasheet. I tried everything I could think of. Here is my QUADSPI init:
hqspi.Instance = QUADSPI;
hqspi.Init.ClockPrescaler = 0;
hqspi.Init.FifoThreshold = 4;
hqspi.Init.SampleShifting = QSPI_SAMPLE_SHIFTING_HALFCYCLE;
hqspi.Init.FlashSize = 23;
hqspi.Init.ChipSelectHighTime = QSPI_CS_HIGH_TIME_2_CYCLE;
hqspi.Init.ClockMode = QSPI_CLOCK_MODE_0;
hqspi.Init.FlashID = QSPI_FLASH_ID_1;
hqspi.Init.DualFlash = QSPI_DUALFLASH_DISABLE;
I would really appreciate some help! thanks