Wait but MCU is unblocked
I haven't been able to wait 500ms without affecting the timers for 7 days.
In this block, doesn't PB14 become "0" after 500ms?
Even if I use comment lines, it doesn't work.
Note: volatile uint32_t Counter = 0;
The "Counter" variable is incremented every 1ms with Timer16.
** STM32F030C6T6 I'm using.
** Own PCB board..
*** Note: Card of a working system.. There is no card design error.
if(htim->Instance==TIM16)
{
Counter++;
if(HAL_GPIO_ReadPin(GPIOC, GPIO_PIN_13)==0)
{
if(HAL_GPIO_ReadPin(GPIOA, GPIO_PIN_2)==0)
{
if(PA10_On==0)
{
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12,GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_14,GPIO_PIN_SET);
Counter=0;
PA10_On=1;
// Tick_PA10_On= HAL_GetTick();
// PA10_On=1;
}
else
{
if(Counter>500) // if((HAL_GetTick()-Tick_PA10_On)>=500)
{
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_14,GPIO_PIN_RESET);
Counter=501;
}
}
}
else
{
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12,GPIO_PIN_SET);
}
}
else
{
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_12,GPIO_PIN_RESET);
}
}