Wake Up from stop mode using USART (HSI for USART Clock,System clock use MSI)
Hi,
I'm using STM32L0 MCU, My system uses MSI as the main system clock, but my USART is to use HSI to be able to wake up from stop mode. My system will enter stop mode for power saving. I am confused about the settings, before enter stop mode, we have to set system clock after STOP mode using HAL API:
__HAL_RCC_WAKEUPSTOP_CLK_CONFIG(RCC_STOP_WAKEUPCLOCK_MSI); // Set system clock as MSI after stop
__HAL_RCC_WAKEUPSTOP_CLK_CONFIG(RCC_STOP_WAKEUPCLOCK_HSI); // Set system clock as HSI after stop so that USART able to wake up the MCU
void PreSleepProcessing(uint32_t *ulExpectedIdleTime) {
*ulExpectedIdleTime = 0; // WFI is called within next function
#ifdef TEST_LP_MODE
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_3, 0);
#endif
if (g_diableStopModeFlags == 0) {
while(__HAL_UART_GET_FLAG(&huart1, USART_ISR_BUSY) == SET); // Make sure that no UART transfer is on-going
while(__HAL_UART_GET_FLAG(&huart1, USART_ISR_REACK) == RESET); // Make sure that UART is ready to receive
HAL_UARTEx_EnableStopMode(&huart1);
// LL_RCC_SetClkAfterWakeFromStop(RCC_STOP_WAKEUPCLOCK_MSI);
// HAL sets STOP wakeup clock for peripherals (so UART on HSI can wake)
__HAL_RCC_WAKEUPSTOP_CLK_CONFIG(RCC_STOP_WAKEUPCLOCK_HSI);
HAL_PWR_EnterSTOPMode(PWR_MAINREGULATOR_ON, PWR_STOPENTRY_WFI);
}
}
Any idea how can I maintain the system clock as MSI after stop mode at the same time USART able to wake up the system from stop mode using HSI?