Skip to main content
Visitor II
September 9, 2024
Question

Weak SPI clock signal at 12MHz on STM32L4A6ZGT

  • September 9, 2024
  • 2 replies
  • 722 views

Below is the analog waveform for the SPI clock at 12MHz. How to improve the strength of this signal and get p-p 3.3V SPI clock at 12MHz ?

"GPIO SPEED" set to the "VERY HIGH" setting. Apart from this, is there any additional settings required ? 

STM 12MHz Analog.png

    This topic has been closed for replies.

    2 replies

    Graduate II
    September 9, 2024

    GPIO speed very high is a good start.

    Have you checked that you are using the correct Mode and Alternate Function for that specific SPIn peripheral?

     

    Visitor II
    September 9, 2024

    Yes all that is configured correctly. Communication works fine at lower frequencies. No problems with SPI other than the strength of the clock signal at 12MHz. 

    Graduate II
    September 9, 2024

    Okay, then check the load next, and remove any loads / connections.