What is the DBATTEN Setting in UCPD_CR register
The DBATTEN setting in the UCPD_CR register claims the following

But as far as I know, the dead battery functionality is always present. It would have to be to work unless this is stored in NVM.
Maybe this DBATTEN is some other Rd value? Maybe the ANAMODE is a proper Rd but this one is a sortof Rd light that is only sufficient to wake the MCU? I can't tell because no information is provided.
If the MCU is powered there is not really a "dead" battery condition. If the MCU is not powered this setting can't take effect.
Any ideas?