Skip to main content
Explorer II
July 17, 2025
Question

When transition from RDP level 1 to RDP level 0, how to avoid a POR ?

  • July 17, 2025
  • 1 reply
  • 337 views

Hello,

MCU: STM32L071

During a transition from RDP level 1 to RDP level 0 the MCU stays stalled.

Only a power supply off then on permits to have it running.

Do you have any suggestion?

Best regards

Mich

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    July 17, 2025

    Hello @mich35 

    As described in the reference manual RM0377

    Note: If the read protection is set while the debugger has been active (through SWD) after last POR (power-on reset), apply a POR (power-on reset) or wakeup from Standby mode instead of a system reset (the option bytes loading is not sufficient).

    Try reload the option bytes after programming, for that you can refer to the "3.8.3 Reloading Option bytes by software"section in the reference manual RM0377.

    mich35Author
    Explorer II
    July 17, 2025

    Hello Imen,

    I was not with the debugger.

    I try to put the system in Standby mode but it does not work, the MCU is stalled. (it works fine from level 0 to level 1)

    I follow "STM32 Security tips - 3 RDP without POR" video (level 0 to level 1) but there is nothing for level 1 to level 0.

    Best regards

    Michel