Skip to main content
Explorer
December 16, 2021
Solved

Where are the schematics for NUCLEO-H743ZI2

  • December 16, 2021
  • 4 replies
  • 3346 views

Hello,

I have here two Nucleos with an H743 on it. If it is rev Y, it is the "old" 144pin Nucleo board with the break-off ST-link board on top. For this there is a schematics in appendix A of the user manual. But if it is rev V, it is NUCLEO-H743ZI2 , note the 2 at the end, with no break-off possibility and a different user manual. And this manual has no schematics included. A trouble start as I start my project. While the manual says PC9 = MCO2 is on CN8 pin4 and CN12 pin1, I see a signal only on CN8 pin4. No way to check what's going on without schematics.

Please ST folks can you provide this somewhere.

Thanks a lot

Martin

    This topic has been closed for replies.
    Best answer by Mike_ST

    Hello,

    MB1137 schematics (NUCLEO-H743ZI) with ST-Link V2 : https://www.st.com/resource/en/schematic_pack/nucleo_144pins_sch.zip

    MB1364 schematics (NUCLEO-H743ZI2) with ST-Link V3 : https://www.st.com/resource/en/schematic_pack/mb1364-h743zi-c01_schematic.pdf

    These links are available at the bottom of the CAD resources page:

    https://www.st.com/en/evaluation-tools/nucleo-h743zi.html#cad-resources

    4 replies

    ST Employee
    December 16, 2021

    Could you share me "which user manual you rely on?"

    Explorer
    December 16, 2021

    Hi Sco,

    yes, sure, here are the manuals I use:

    For the "old" 144pin Nucleo I have UM1974, page footer says DocID028599 Rev 7 December 2017

    For the NUCLEO-H743ZI2 I have UM2407, page footer says UM2407 Rev 2, June 2020, which I downloaded just yesterday. This is the one I desire schematics for.

    I hope you can help.

    Martin

    Mike_STAnswer
    Technical Moderator
    December 16, 2021

    Hello,

    MB1137 schematics (NUCLEO-H743ZI) with ST-Link V2 : https://www.st.com/resource/en/schematic_pack/nucleo_144pins_sch.zip

    MB1364 schematics (NUCLEO-H743ZI2) with ST-Link V3 : https://www.st.com/resource/en/schematic_pack/mb1364-h743zi-c01_schematic.pdf

    These links are available at the bottom of the CAD resources page:

    https://www.st.com/en/evaluation-tools/nucleo-h743zi.html#cad-resources

    Graduate
    January 15, 2024

    Hello,

    I bought one Nucleo-H743ZI2 board and found the two capacitors (C71 and C72) for X2 32.768KHz are not installed. May I know if I need to install them with 5.1pF if I want to use the X2? I went through the manual "UM2407 User manual for STM32H7 Nucleo-144 boards (MB1364)". But it seems not mention the two capacitors for the LSE clock. Thank you.32.768.PNG

     

    Technical Moderator
    January 15, 2024

    Hello @Jiaming  and welcome to the community.

    This thread is already closed and I suggest you to open a new one.

    Thank you for your understanding.

    Explorer
    December 16, 2021

    Hi Mike,

    thanks for this quick and complete answer - both thumbs up

    Martin