Skip to main content
Visitor II
October 6, 2015
Question

Where does the automatically downloaded STM32CubeMX update go?

  • October 6, 2015
  • 8 replies
  • 1816 views
Posted on October 06, 2015 at 20:59

I noticed that there was a new CubeMX version available 4.10.1.  The Cube SW downloaded it semi automatically but I can't find it.

It was unzipped automatically but not installed. So where is it.

I have a Windows 7 machine
    This topic has been closed for replies.

    8 replies

    Visitor II
    October 7, 2015
    Posted on October 07, 2015 at 11:48

    For me, every time, I did an automatic update of STM32CubeMX, it dis not work afterwards anymore (exe missing).

    So I always download and install it manually.

    Visitor II
    October 7, 2015
    Posted on October 07, 2015 at 13:41

    Hi guys,

    After launching thedowload of the new version 4.10.1 within ''Check Update Manager'':

    1-Close CubeMx

    2-Click right on its shortcut

    3-Click on ''Run as administrator''

    Then, updates will be installed completely.

    -Shahrzad-

    LMI2Author
    Visitor II
    October 21, 2015
    Posted on October 21, 2015 at 23:49

    Tonight I did exactly like it was told below. But nothing happened. Or is it very slow or something?

    Graduate II
    October 21, 2015
    Posted on October 22, 2015 at 00:46

    Do you have any AV software that might be interfering with normal operation of the computer?

    LMI2Author
    Visitor II
    October 22, 2015
    Posted on October 22, 2015 at 16:46

    Heh. I have an antivirus suite from F secure. But I think this machine works quite normally (for a Microsoft product that is). That was a joke, everything works, no freezes or other problems. I can install drivers and so on. And CCleaner and so on are able to update themselves (if I let them). But for the next update I will try taking off the AV suite for awhile.

    Visitor II
    October 23, 2015
    Posted on October 23, 2015 at 23:19

    I have also experience the same issue but have another issue as well.

    I downloaded the latest STM32CubeMX installer directly (not as an update within STMCube) and ran the installer with Administrative permissions.

    I then attempted to start the application using ''Run as Administrator'' and received the message in the attachment.

    Clive - How do I resolve this? What have I missed in the installation??

    Eric

    ________________

    Attachments :

    STM32CubeMX_update_Issue.PNG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtgU&d=%2Fa%2F0X0000000aVi%2F4VnVjEd..NikriA5cYu7A3c0BRohA2A0_mYMC0MSMsk&asPdf=false
    Graduate II
    October 23, 2015
    Posted on October 24, 2015 at 01:37

    Not really my battle.

    I guess I'd look at the ownership/rights for the directories in question, and if they in fact exist. Files that are running (.EXE/.DLL) can't be deleted if the system has them loaded.

    Be very sure there aren't multiple instances of the software running, double check in the Task Manager.

    Visitor II
    October 27, 2015
    Posted on October 27, 2015 at 17:32

    Hi  apperley.eric.001,

    Make sure of your administrator rights in the STM32CubeMx folder. Maybe it is the cause of the problem.

    -Shahrzad-

    Visitor II
    March 19, 2024

    Really? This is all you have to give as an answer? I'm running this out of an Command Prompt in Administrator mode and I get this same message.