Whether flow control byte is needed in the SPI frame for STM32F407?
Hi,
There is a STM32F407 on my board to configure and control the optical module. Also, STM32F407 use SPI to interface with CPU. STM32F407 work as SPI slave mode, and CPU work as master mode. Some protocol require one flow control byte in SPI timing, such as OIF protocol. My understanding is :
For read operation. After slave receive the operation code and address, slave need time to prepare data according to address then put the data into TX_Buffer. This all will be finished in the one clock period as below red mark shown. If slave can't finish the job in time, slave must inform to host through flow control byte .

My question is whether flow control byte is needed in the SPI frame for STM32F407?or it can mitigate this issue through reducing the SCK frequency, not through flow control byte?
Thanks in advance!
Best regards!
Jason