Which TIMs support Quadrature encoder
Hello,
I am trying to use the quadrature encoder mode of the TIM in the STM32U585VITx, for positioning purposes of a stepper motor movement.
According to DS13086, page 79, the general purpose timers (TIM2, TIM3, TIM4, TIM5, TIM15, TIM16, TIM17) support quadrature encoders.
However, according to RM0456 Rev 5, page 2083, TIM 1.8 has support for quadrature encoders.
Could you please clarify which TIMs support this encoder?
Also, I am currently trying to use TIM8 for this purpose (not sure if it is the right timer), but when I move the motor and read the timer, I just get a bunch of zeros.
Any help would be greatly appreciated,
Thank you