Why does PA4 chip select not stay high when configuring PUPDR pull-up on STM32F407VGTX?
Hi,
I’m working with the STM32F407VGTX and I am using GPIO PA4 as the SPI chip-select (CS) pin. In my GPIO initialization, I set the PUPDR register to configure PA4 with a pull-up, expecting the CS pin to remain HIGH when idle. However, I observe on my logic analyzer that after initialization PA4 goes HIGH briefly, then returns LOW (its default state) even though the pull-up is set. I am attaching a screenshot of my logic analyzer for reference.
Could anyone please explain why the pin doesn’t remain high with the pull-up configuration, and what’s the correct way to configure PA4 so that CS is HIGH when SPI is not active?
Thank you!