Why OTG_HS USB/USBX Host on STM32U5Axx just does not work? (2)
I encountered a problem while desperately trying to make USB OTG_HS Host configured on a new Nucleo-U5A5ZJ-Q using CubeMX and ThreadX+USBX. I know that this board is not designed to provide USB power, but this can be overcome with undocumented SB8-10 jumpers and UCPD is not an issue here. I am also aware that at the beginning of the HAL_HCD_MspInit() function __HAL_RCC_SYSCFG_CLK_ENABLE(); line needs to be added.
After several evenings of research (see here) I think I nailed down the problem to USB_HostInit() function.
At the end of this function, host mode events are enabled using GINTMSK register (RM0456, section 73.14.8 OTG interrupt mask register [alternate] (OTG_GINTMSK), offset 0x18).
USBx->GINTMSK |= (USB_OTG_GINTMSK_PRTIM | USB_OTG_GINTMSK_HCIM | \
USB_OTG_GINTMSK_SOFM | USB_OTG_GINTSTS_DISCINT | \
USB_OTG_GINTMSK_PXFRM_IISOOXFRM | USB_OTG_GINTMSK_WUIM);
The problem I found and cannot explain is that after when this line is executed, GINTMSK register value is still zero. Other OTG_HS registers get correctly set so probably the problem is NOT caused by misconfigured or not enabled RCC AHB2 peripheral clock (RM0456, 11.8.30 RCC AHB2 peripheral clock enable register 1, bits 14 & 15 - OTGEN & OTGHSPHYEN flags).
Please advise, I start to suspect some hardware bug or incorrect GINTMSK register offset.
Probably a separate issue is that GAHBCFG.GINTMSK register flag is not set (Global interrupt mask, RM0456, 73.14.3).
The second screenshot presents OTG_HS-related registers' state after when MX_USB_OTG_HS_HCD_Init() function was finished and HAL_HCD_Start() function was called.