Skip to main content
Explorer
May 10, 2024
Question

Wrong values getting assigned when same structure assignment is done.

  • May 10, 2024
  • 1 reply
  • 918 views

I am developing an TCP/IP Server Client application on my NUCLEO-F207ZG  development board.I am implementing a function to send ADC values on Ethernet.

void Client_Data_Send(void)
{
char temp_buff[TEMP_BUFF_SIZE];
volatile uint32_t buff_len;
volatile uint16_t Temperature = 0;
struct pbuf *p = NULL;

Temperature = TEMP;

buff_len = sprintf(temp_buff,"DHT11 Sensor value from TCP Client : %u \n\r",Temperature);

/*allocate pbuf from ram*/
p = (pbuf_alloc(PBUF_TRANSPORT,buff_len,PBUF_POOL));

(tcp_client->p)= (p);

if(tcp_client->p != NULL)
{
/*copy the data to send into the allocated pbuf*/
pbuf_take( tcp_client->p ,(char *)temp_buff,buff_len);

/*send data*/
tcp_client_send(tx_pcb, tcp_client);

/*free mem*/
pbuf_free( tcp_client->p);
}

}

Above is the function I implemented.

At line (tcp_client->p)= (p); when I debuged I came to know that values are not getting assinged.

Below are the screen shot.

pradeepwagre_0-1715353161045.png

pradeepwagre_1-1715353190355.png

since wrong values for all members getting assigned I am facing Hard fault issue. Is it structure alignment issue? I am using LwIP library for Tcp/Ip application.

 

    This topic has been closed for replies.

    1 reply

    ST Employee
    May 23, 2024

    Hello @pradeepwagre ,

    At first glance this code seems to have some issues and it is not conformed to the guidelines of implementation with LWIP on STM32s.

    You can follow this User Manual Developing applications on STM32Cube with LwIP TCP/IP stack
    to get more info bout the way to use LwIP tcp/ip stack.
    you can check the way to use LwIP either with or without Rtos and take this following example as reference.

    STM32CubeF2/Projects/NUCLEO-F207ZG/Applications/LwIP/LwIP_HTTP_Server_Netconn_RTOS at master · STMicroelectronics/STM32CubeF2 (github.com)

    You can also implement and example using LwIP without RTOS by following this Application Note (see section 4.1.2) in which we implement a periodic process in While(1) loop.

    BR