Skip to main content
Visitor II
December 16, 2025
Question

X-NUCLEO-PLM01A1: ST7580 TX/RX not continuous, no data reception, TX_ON/RX_ON LEDs not blinking

  • December 16, 2025
  • 1 reply
  • 76 views

Hello,

I am working with two X-NUCLEO-PLM01A1 PLC expansion boards, each connected to a different STM32 MCU board.

Hardware setup:

  • Transmitter MCU: STM32C092CBT6

  • Receiver MCU: STM32G070CBT6

  • PLC modem: ST7580 on both X-NUCLEO-PLM01A1 boards

  • Both boards are connected over the same power line

Problem description:

  • I am trying both DL mode and physical data transmission.

  • Data transmission is not continuous.

  • The receiver board does not receive correct data (data is corrupted or not received).

  • The TX_ON and RX_ON LEDs on both X-NUCLEO-PLM01A1 boards remain LOW and do not blink during transmission or reception.

  • The ST7580 IC replies on SPI/UART, but no proper PLC data transfer occurs.

Additional observation:

  • I also tried using the ST-provided API / middleware available on the ST website, but the transmission gets stuck with a transmission error and does not complete successfully.

Observations:

  • SPI/UART communication between MCU and ST7580 is working.

  • T_REQ behavior has been checked.

  • Despite transmission attempts, TX_ON and RX_ON LEDs never indicate activity.

Questions:

  1. What are the possible reasons for TX_ON and RX_ON LEDs staying LOW?

  2. Are there any mandatory ST7580 configuration registers that must be set for continuous transmission?

  3. Are there known issues or differences when using different MCU families (STM32C0 vs STM32G0) with X-NUCLEO-PLM01A1?

  4. Is there any recommended initialization or timing sequence required before starting DL or physical data transmission?

  5. Could this be related to line coupling, impedance, or hardware configuration on the X-NUCLEO-PLM01A1?

  6. Are there any known limitations or required adaptations when using the ST7580 API on non-reference MCU boards?

Any guidance, reference designs, or example configurations would be very helpful.

Thank you in advance.

 

WhatsApp Image 2025-12-16 at 09.59.05.jpeg

    This topic has been closed for replies.

    1 reply

    Super User
    December 16, 2025

    This is a duplicate of your previous question:

    STM32C092 + X-NUCLEO-PLM01A1: UART TX works interm... - STMicroelectronics Community

     

    Please don't repost the same question. You got engagement there, perhaps follow up to add more relevant details.

    Midhul_PkAuthor
    Visitor II
    December 16, 2025

    Okay, but I couldn’t get proper replies. That’s why I posted it again.

    Super User
    December 18, 2025

    @Midhul_Pk wrote:

     I couldn’t get proper replies. That’s why I posted it again.


    You haven't answered questions, and haven't provided details requested:

    1. A diagram of your setup.
    2. Full part numbers of the stuff you are using.
    3. Details of what investigation/debugging you have done.
    4. Have you tried known-good examples

    Just repeating the same question without providing requested information isn't going to get better answers.

    How to write your question to maximize your chances to find a solution

    Getting faster and better answers in the community

     

    Note that ST have recently added an AI chatbot - might be worth giving it a try:

    STM32 Sidekick: the AI-powered tool that accelerates your design journey

    How to use STM32 Sidekick