Skip to main content
Visitor II
May 29, 2024
Question

Zero crossing detection

  • May 29, 2024
  • 2 replies
  • 1421 views

HELLO, 

Can you please suggest us any mcu having internal block for zero crossing detection in stm32 for 50 - 60hz frequency signals or any slave chips that are dedicated for zero crossing detection.

 

Thank you, 

Krishna. 

 

    This topic has been closed for replies.

    2 replies

    Technical Moderator
    May 29, 2024

    Welcome @Krishna36, to the community!

    This is a recurring question for which you will find several entries here in the community, e.g. this one.

    Hope that helps?

    Regards
    /Peter

    Graduate II
    May 29, 2024

    How large is your 50 Hz? What is your timing requirement?

    Probably you can use a STM32 with comparator and use the 50 Hz offset to about half the supply voltage compared to half the supply voltage. I would use an external comparator with common mode input to some - 100 mV put a fitting resistor in the 50 Hz line, clip the voltage with two antiparallel schottky diode and compare against ground.