Skip to main content
Lead
March 24, 2024
Question

CC1 and CC2 - Do I need them for STM32MP157?

  • March 24, 2024
  • 1 reply
  • 1109 views

I'm going to build my own computer by using STM32MP157 and install OpenSTLinux onto it. 

The powering for STM32MP157 can be done via USB-C connection, but that requires an USB-C charger of 5 volts.

Can I skip that and only using a regular charger like 3.5 DC jack? I know that there are two pins that are connected to STM32MP157 processor. They are USB_PWR_CC1 and USB_PWR_CC2. They are connected to PA5 and PA4 at the processor.

Who is using these pins? Is it the OpenSTLinux? 

Do I really need them?

 

 

Skärmbild 2024-03-24 150039.png

This topic has been closed for replies.

1 reply

PatrickF
Technical Moderator
March 26, 2024

HI @DMårt 

CC1 and CC2 lines are used to detect the charger capabilities and uBoot will issue a message and blink red led.

This could be disabled in Device Tree if you are not using USB Type-C to power the board (or if you don't need such check).

See STM32MP157F-EV1 board for an example of 5V DC Jack power supply.

See also this rather old post on similar subject https://community.st.com/t5/stm32-mpus-boards-and-hardware/my-stm32mp157f-dk2-is-powered-by-5v-3a-psu-but-at-the-boot-up/m-p/211923

Regards

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here