Skip to main content
Associate III
January 15, 2025
Solved

Developer package link broken

  • January 15, 2025
  • 2 replies
  • 706 views

Hello,

 

I am having an issue when I try to download the Developer package in the wiki. I am using this link (https://wiki.st.com/stm32mpu/wiki/STM32MPU_Developer_Package#Installing_the_Starter_Package) in the 5.2 section, there, it redirects me to (https://www.st.com/en/embedded-software/stm32mp1dev.html#get-software). In the last link, when I try to download the file, it downloads the wrong file, since it downloads the SDK instead of the Developer package. Probably there is an error in the API and it gets the wrong file. Does anyone else experiences the same issue?

Best answer by Pwxn

Hello @obedPH,

 

When you click on the download link, you should select the MP1/2-DEV-SRC and download the latest.

I tried on my side and I could download the developer package without any issue : en.SOURCES-stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06.tar.gz

 

The other link are for software development kit specific for each architecture. 

 

I hope this help you.

 

Regards,

2 replies

Pwxn
PwxnBest answer
ST Employee
January 16, 2025

Hello @obedPH,

 

When you click on the download link, you should select the MP1/2-DEV-SRC and download the latest.

I tried on my side and I could download the developer package without any issue : en.SOURCES-stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06.tar.gz

 

The other link are for software development kit specific for each architecture. 

 

I hope this help you.

 

Regards,

obedPHAuthor
Associate III
January 17, 2025

Hello @Pwxn ,

Yes, it worked now, thank you for the reply,

 

 

Regards