Skip to main content
Associate II
May 26, 2024
Solved

Enable ethernet clock on both A7 and M4

  • May 26, 2024
  • 1 reply
  • 1027 views

Dears,

I'm using STM32MP151 and have a uncertain quesion.

In my cases, Both A7 and M4 need to access the register ETH_MACSTSR and ETH_MACSTNR to get time stamp.

It's required to enable the ethernet clock on both side before accessing these registers, i.e. the bit7 in RCC_MP_AHB6ENCLRR and RCC_MC_AHB6ENCLRR.

It seems workable now. But I'm not sure whether it have any potential problem.

If this method is not practical, do you have any suggestions? 

Thanks

Regards,

 

 

 

 

Best answer by PatrickF

Hi @fantasylsdo 

Yes, I assume you want to overcome the fact that Linux will stop the AHB bus clock going to ETH whenever no register access is needed on their side.

To do that, you could set ETHMACEN bit in RCC_MC_AHB6ENSETR to keep clock when Linux release the peripheral.

As you are accessing read-only registers, there is no potential issue foreseen (except if huge amount of read from MCU side could create real time issue on Linux driver when accessing ETH register).

Keep in mind that accessing a peripheral from two processors is not an usual use and should always be used with care.

Regards.

1 reply

PatrickF
PatrickFBest answer
Technical Moderator
May 31, 2024

Hi @fantasylsdo 

Yes, I assume you want to overcome the fact that Linux will stop the AHB bus clock going to ETH whenever no register access is needed on their side.

To do that, you could set ETHMACEN bit in RCC_MC_AHB6ENSETR to keep clock when Linux release the peripheral.

As you are accessing read-only registers, there is no potential issue foreseen (except if huge amount of read from MCU side could create real time issue on Linux driver when accessing ETH register).

Keep in mind that accessing a peripheral from two processors is not an usual use and should always be used with care.

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here
Associate II
October 6, 2024

Thanks for your kind reply. It helps a lot.