Skip to main content
mikesponk2
Associate III
September 6, 2023
Question

Enabling the GPU on a DPI panel

  • September 6, 2023
  • 1 reply
  • 1801 views

Hi, I have a custom board with a parallel RGB display connected to it that works OK when using pixman.

If I enable the galcore.ko module, weston fails;

 

 

[15:27:38.101] weston 10.0.0
https://wayland.freedesktop.org
Bug reports to: https://gitlab.freedesktop.org/wayland/weston/issues/
Build: 10.0.0
[15:27:38.102] Command line: /usr/bin/weston --modules=systemd-notify.so --log=/home/weston/weston.log
[15:27:38.102] OS: Linux, 5.15.67, #14 PREEMPT Mon Sep 4 17:47:46 CEST 2023, armv7l
[15:27:38.102] Flight recorder: enabled
[15:27:38.103] Using config file '/etc/xdg/weston/weston.ini'
[15:27:38.103] Output repaint window is 10 ms maximum.
[15:27:38.104] Loading module '/usr/lib/libweston-10/drm-backend.so'
[15:27:38.121] initializing drm backend
[15:27:38.121] Trying logind launcher...
[15:27:38.166] logind: session control granted
[15:27:38.195] using /dev/dri/card0
[15:27:38.195] DRM: supports atomic modesetting
[15:27:38.195] DRM: supports GBM modifiers
[15:27:38.195] DRM: supports picture aspect ratio
[15:27:38.196] Loading module '/usr/lib/libweston-10/gl-renderer.so'
[15:27:38.268] EGL client extensions: EGL_EXT_client_extensions
EGL_EXT_platform_base EGL_KHR_platform_wayland
EGL_EXT_platform_wayland EGL_KHR_platform_gbm
[15:27:38.268] failed to initialize display
[15:27:38.268] EGL error state: EGL_NOT_INITIALIZED (0x3001)
[15:27:38.268] failed to initialize egl
[15:27:38.269] BUG: layer_list is not empty after shutdown. Calls to weston_layer_fini() are missing somwhere.
[15:27:38.269] fatal: failed to create compositor backend

 

 

So it seems that the eglInitialize() function fails.

 

The galcore module is loaded OK:

 

 

[ 23.272361] galcore: loading out-of-tree module taints kernel.
[ 23.308976] Galcore version 6.4.9.436021

 

 

With the modetest application I see the correct pagttern on the display

The kmscube application fails:

 

 

root@stm32mp1:~# kmscube
[ 1] HAL user version: 6.4.13.608341
[ 2] HAL kernel version: 0.0.0.0
[ 3] HAL user version: 6.4.13.608341
[ 4] HAL kernel version: 0.0.0.0
[ 5] ioctl(DRM_IOCTL_GEM_CLOSE) failed
)
[ 6] HAL user version: 6.4.13.608341
[ 7] HAL kernel version: 0.0.0.0
[ 8] HAL user version: 6.4.13.608341
[ 9] HAL kernel version: 0.0.0.0
[ 10] ioctl(DRM_IOCTL_GEM_CLOSE) failed
)
failed to create gbm surface
failed to initialize GBM

 

 

 

I have not found information about how to enable debug on the egl modules.

Anyone has any idea about how to debug such a situation?

Many thanks

 

 

1 reply

ST Employee
September 13, 2023

Hi,

I did the test myself and indeed I had a problem when activating galcore.

To make it work, I had to use the config file of the starter package.

So I think you can start from this config file and then make your modifications on top of it.

don't hesitate to come back to me if needed .

Regards,

Grégory

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Visitor II
June 1, 2025

Can you explain in detail which configurations it is