Skip to main content
Associate III
October 10, 2024
Solved

Error message inquiries and display problems

  • October 10, 2024
  • 1 reply
  • 2186 views

Hello, I developed a custom board with a pinmap based on stm32mp157f - dk2.

I think if you match the pinmap and use the start package, lcd and other features will work.

I re-created the sd card according to that advice, and I also rebooted it, but the same thing is happening.

What should I do?

LeeJaewon_0-1728536466946.png

History: https://community.st.com/t5/stm32-mpus-products/error-message-inquiries-and-display-problems/m-p/714459#M11850

https://community.st.com/t5/stm32-mpus-boards-and-hardware/check-error-code-for-uart4/td-p/700161

 

 

Best answer by PatrickF

Hi @LeeJaewon 

"devil is in the details".

I think you should check what you made different versus stm32mp157F-dk2 board. Unless you are really insightful of the system, even very small board change could lead to a blocking point.

Are you using exactly same STPMIC1 and supply usage ? USB Type-C supply with ADC connections ? Ethernet PHY, etc...

Custom board is usually meaning custom device tree and need to build complete image.

STM32MP157F-DK2 image are not build with other boards binary compatibility in mind.

Regards.

 

1 reply

PatrickF
PatrickFBest answer
Technical Moderator
October 10, 2024

Hi @LeeJaewon 

"devil is in the details".

I think you should check what you made different versus stm32mp157F-dk2 board. Unless you are really insightful of the system, even very small board change could lead to a blocking point.

Are you using exactly same STPMIC1 and supply usage ? USB Type-C supply with ADC connections ? Ethernet PHY, etc...

Custom board is usually meaning custom device tree and need to build complete image.

STM32MP157F-DK2 image are not build with other boards binary compatibility in mind.

Regards.

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here