Skip to main content
Visitor II
September 30, 2024
Question

ESDALC6V1-5M6, LD39150PU33R ibis file

  • September 30, 2024
  • 2 replies
  • 537 views

Hello forum;

I needed help to do some SI simulation on ESDALC6V1-5M6 and LD39150PU33R Hyperlynx/Altium Designer SI simulator. Hence my question is does this ibis model exist? If yes where can I download it?

 
 

 

2 replies

PatrickF
Technical Moderator
October 1, 2024

Hi,

I fear IBIS are not available for ESD protection devices. Maybe a simple hand-made model could be used (using the information in product datasheet).
For LDOs, I wonder what could be the link with high-speed signal integrity simulation. I guess IBIS model does not apply at all power devices like LDOs.

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here
Visitor II
October 1, 2024

You can use Altium designer. You can manually add parasitic parameters (like capacitance, resistance, and inductance) for ESD components.