Skip to main content
Uusta.1
Associate III
November 21, 2021
Solved

How can I use Stm32mp157c-dk2 with 7inch HDMI LCD(B)

  • November 21, 2021
  • 2 replies
  • 2090 views

Hi, I want to use my stm32mp157c-dk2 board with capacitive touchscreen display(7inch HDMI LCD (B)), image that I installed for stm32mp1 board is Distribution Package st-example-image-qt (DISTRO=openstlinux-eglfs MACHINE=stm32mp1-disco source layers/meta-st/scripts/envsetup.sh)

7inch HDMI LCD(B)

I think I need to modify device tree and kernel configuration but I dont know which drivers do I need, could you help me?

This topic has been closed for replies.
Best answer by Uusta.1

Update: power supply for my stm32mp157c-dk2 board was not enough, after I changed my power suppy, my hdmi screen is working

2 replies

PatrickF
Technical Moderator
November 22, 2021

Hi,

For display, did you tried with out of the box DK2 Starter Package ?

More info on https://wiki.st.com/stm32mpu/wiki/How_to_display_on_HDMI

For touch, as it is using usb, likely some driver should be added if default HID driver are not enough (DK2 with started package already work with many usb peripherals such as mouse, keyboard, webcam, etc...).

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here
Uusta.1
Uusta.1AuthorBest answer
Associate III
November 22, 2021

Update: power supply for my stm32mp157c-dk2 board was not enough, after I changed my power suppy, my hdmi screen is working

PatrickF
Technical Moderator
November 22, 2021

Hi,

nice to see you succeeded to get your HDMI display working.

Notice that the 5V output on HDMI connector is limited by a polyswitch fuse and should be limited to somewhat 200mA.

For USB Type-A, the limitaition is 500mA.

I'm not sure your display is powered thru USB and/or HMDI, but ensure not using more power in case back-light is at maximum.

Regard

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here