Skip to main content
HKim.23
Associate III
July 26, 2021
Solved

How to get terminal on STM32MP157D-EV1? The COM port cann't be seen from the host PC.

  • July 26, 2021
  • 3 replies
  • 2222 views

The board is set up as follows, and USB of ST-Link V2-1 is connected to Host PC.

0693W00000D0cO8QAJ.jpg 

0693W00000D0cJOQAZ.jpg 

when using Linux host pc , /dev/ATM* devices not recognized.

So I used a Windows PC, but it is not recognized either.

Do I need to install a special driver to recognize the Uart serial?

Or is there a problem with the Jumper setting?

This topic has been closed for replies.
Best answer by HKim.23

Oh ~~~~~~~~~ Sorry,,,

JP1 must be removed.

3 replies

HKim.23
HKim.23AuthorBest answer
Associate III
July 26, 2021

Oh ~~~~~~~~~ Sorry,,,

JP1 must be removed.

HKim.23
HKim.23Author
Associate III
July 26, 2021

Closed...

JKim.2
Associate III
March 16, 2023

Hello,

I set the jumpers same (JP1 removed, JP4[2-3], JP5[2-3]). However, when I connect the USB cable from CN4(ST-Link V2-1) to PC, the results are still same as yours. (Linux host pc: /dev/ttyACM* devices not recognized. Windows PC: the USB is not recognized either.) Do I need any other driver or accessory for this?

Thanks.

PatrickF
Technical Moderator
March 16, 2023

Hi,

what is the status of LD6 ?

Check your USB cable, there is some USB cables (provided with cheap gadgets) which does not have USB data connected (only VBUS wires) !

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here
JKim.2
Associate III
March 16, 2023

Hi,

LD6 is off.

I tried other 3 USB cables. They are all the same.

Thanks.