Associate III
January 9, 2023
Question
How to properly intiate boot sequance of stm32mp1?
- January 9, 2023
- 4 replies
- 6306 views
I am upgrading from ecosystem 4.1 to 4.0. after changing every thing properly in the device tree. and now i successfully compiled the image partitions using bitbake how ever when i boot using the flashed images every thing works correctly utill i recive the following error on the boot
Starting version 250.5+
root '/dev/disk/by-partuuid/e91c4e10-16e6-4c0e-bd0e-77becf4a3582' doesn't exist or does not contain a /dev.the full boot log is in the following .txt file
i did try to flash using :
- the script provided to prepare a raw image
- manually using fdisk and dd
- change the config in boot Partion and insert the rootfs adiquet id
- verify the UUID of the partition
the compilation generates the following message when i compile the image using bitbake
NOTE: Started PRServer with DBfile: /media/user1/st4_1/kirkstone/build-openstlinuxweston-stm32mp1/cache/prserv.sqlite3, Address: 127.0.0.1:37179, PID: 2053248
Loading cache: 100% |###########################################| Time: 0:00:05
Loaded 4455 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies
Build Configuration:
BB_VERSION = "2.0.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "universal"
TARGET_SYS = "arm-ostl-linux-gnueabi"
MACHINE = "osd32mp1-brk"
DISTRO = "openstlinux-weston"
DISTRO_VERSION = "4.0.4-snapshot-20230108"
TUNE_FEATURES = "arm vfp cortexa7 neon vfpv4 thumb callconvention-hard"
TARGET_FPU = "hard"
DISTRO_CODENAME = "kirkstone"
GCCVERSION = "11.%"
PREFERRED_PROVIDER_virtual/kernel = "linux-stm32mp"
meta-python
meta-oe
meta-gnome
meta-initramfs
meta-multimedia
meta-networking
meta-webserver
meta-filesystems
meta-perl = "HEAD:05dcac98473402d87e0af73bbc2c5a6a840abe93"
meta-st-stm32mp = "HEAD:ca501bd7dbe023682903ceedddaacd940b0898f4"
meta-qt5 = "HEAD:5b71df60e523423b9df6793de9387f87a149ac42"
meta-st-openstlinux = "HEAD:cb736b403d0fef2a02390695613b6b4bb13ca1b7"
meta = "HEAD:f7766da462905ec67bf549d46b8017be36cd5b2a"
meta-octavo-osd32mp1-kirkstone = "<unknown>:<unknown>"
Initialising tasks: 100% |######################################| Time: 0:00:11
Sstate summary: Wanted 1276 Local 196 Mirrors 0 Missed 1080 Current 1824 (15% match, 65% cSetSetscenWARNING: octavo-image-weston-1.0-r0 do_image_complete: Missing 'EULA_FILE_ST' var : no image license copied...
WARNING: octavo-image-weston-1.0-r0 do_st_write_license_create_summary: IMG LIC SUM: File does not exist with open file /media/user1/st4_1/kirkstone/build-openstlinuxweston-stm32mp1/tmp-glibc/deploy/images/osd32mp1-brk/octavo-image-weston-openstlinux-weston-osd32mp1-brk.license
WARNING: octavo-image-weston-1.0-r0 do_st_write_license_create_summary: IMG LIC SUM: File does not exist with open file /media/user1/st4_1/kirkstone/build-openstlinuxweston-stm32mp1/tmp-glibc/deploy/licenses/st-image-resize-initrd-openstlinux-weston-osd32mp1-brk-20230108193424/package.manifest
NOTE: Tasks Summary: Attempted 7537 tasks of which 5142 didn't need to be rerun and all succeeded.
NOTE: Writing buildhistory
NOTE: Writing buildhistory took: 8 secondswhat should i do to make this boot properly ?