Incorrect I2C addresses in MB1854 (B-CAMS-IMX) schematics for IMU and ToF sensors
Hello,
There seems to be an issue with the I2C addresses listed in the MB1854 (B-CAMS-IMX) documentation and schematics (B01/B02).
The documents show:
- IMU: 0xD4 / 0xD5
- ToF: 0x52
However, these appear to be 8-bit addresses. The correct 7-bit I2C addresses should be:
- ToF (VL53L5CX): 0x29
- IMU (ISM330DLC): 0x6A / 0x6B
This can cause confusion when using standard I2C tools or drivers.
Could you please clarify or update the documentation to specify the address format (7-bit vs 8-bit)?
Thanks.