Hi @damien1 ,
on a pure RAM, no matter the data bus swapping (bits within a byte or bytes Vs bytes), your read what your have written. So, no need to configure any HW/SW about this.
Obviously, in case of bytes swap, DQS/DQM should follow their byte.
There is anyway some restriction on byte and but swapping (e.g. D0-D7 on LPDDR2/3 should be on byte0 without any bit swap) as data bus could also carry access to memory internal config/status registers.
On DDR3/DDR3L, all data swaps are allowed because writting memory register is done using address bus as data (which is not the case on LPDDR).
Regards,
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.