Skip to main content
Visitor II
December 27, 2023
Question

Issue regarding DDR3

  • December 27, 2023
  • 1 reply
  • 955 views

Hello

  • I'm using stm32mp157aaa3 processor in our custom board.And I'm working on DDR3L with arm-trusted-firmware(V2.5) ddr3 routines as my reference code and reference manual(RM0436) and Application not(AN5168).
  • When I am hard-coding the register values in arm-trusted-firmware it works fine which means my hardware is working fine,but when I'm porting the same code to bare-metal we couldn't read and write the ddr memory location and the ddr memory is not released.
  • And I have also tried STM32DDRFW-UTILS.And here too i get the same issue.
  • Could you please suggest me a way on how to assign memory size for ddr3l and release ddr memory in bare-metal and how to resolve the read and write issue.

 

 

Thanks&Regards

Akshitha

 

This topic has been closed for replies.

1 reply

PatrickF
Technical Moderator
January 3, 2024

Hi @pattem_09 

Did you use STPMIC1 ? Is the related DDR3L supplies enabled (and reference/termination supplies if used) ?

Did you have setup the DDR clock in right way (PLL and HSE bypass or crystal) ?

Is there activities on DDR pins (CLK, CKE, etc...)?

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here